Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly Arrangements in NX11 manufacturing

Creator
Creator

Good morning everyone,

 

NX11 manufacturing turning. I am turning a shaft in our DMG NLX2500SY and I need to start the process with the end of the shaft 4.0 from the face of the chuck jaws to face and drill. Then I need to advance the stock 7.0 and machine a groove and mill a key. Can I use assembly arrangements to position the part in two different places in manufacturing instead of using two separate linked bodies or two MCS?

 

Thanks

 

Tim

2 REPLIES 2

Re: Assembly Arrangements in NX11 manufacturing

Legend
Legend
Hello Tim,

I advise you not to do so. Switching the Arrangements will trigger design change events to your operations and then they want to regenerate.
Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Re: Assembly Arrangements in NX11 manufacturing

Creator
Creator

I was afraid of that. Thanks for the info

Learn online





Solution Information