Cancel
Showing results for 
Search instead for 
Did you mean: 

Assign nc axis C4 to channel 1 and 2 in CSE driver

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,

Would anyone advise me how to add in CSE nc axis C4 to both channel 1 and 2? I have the M45 connection of the C-axis according to the channel used. I need to assign an axis to both channels when milling on Channels 1 and 2.

Thank you

 

M45.PNG

1 REPLY

Re: Assign nc axis C4 to channel 1 and 2 in CSE driver

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

than need to be done inside the kinematics model in the MTB.

 

As the spindles C4 can/need be assigned to both channels.
"Channel Configuration" Make sure C4 is in both channel as "Referenced Spindles"

 

As an axis (interpolation) it is possible to assign it to one channel only, but this is the initial state at start of simulation."Assigned Axis"

 

When during simulation a different channel will use these axis it first need to be removed from the initial channel and assigned to the desired channel.

 

Check the CSE commands:

  • AttachJoint
  • DetachJoint
  • RetrievJoint

In the Sinumerik CCF it is implemented in GET and GETD

 

Hope it helps

Thomas

 

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information