Cancel
Showing results for 
Search instead for 
Did you mean: 

Automatic updated Feeds and Speeds

Valued Contributor
Valued Contributor

Hi,

 

when generating my operations autmatically from the MKE, I have

defined my feed and speeds. The settings which I have setted are also

included. I would like that the calculation is updated aumatically without

calculating them like here - is that possible ?

 

Thank you Smiley Happy

snip_20170829110158.png

 

 

 

 

 

 

NX 11.0.1.11
3 REPLIES

Re: Automatic updated Feeds and Speeds

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Muddi_91,

 

thank you for your question.

 

2017-08-29 11_25_48-NX 12 CAM_nx1201 Build CAM_nx1201.127 - Manufacturing.png

 

Please be aware that your Machining Data Library has to be up to date, otherwise you will get warning messages stating that data input is missing and an automatic update isn't possible.

 

If you have any further questions on this topic, please let us know.

 

Cheers,

Alexander

Re: Automatic updated Feeds and Speeds

Genius
Genius

Hi Muddi, 

 

How have you defined your feeds and speeds in the MKE?

 

If you are using custom Machining Data Libraries you can do it as Alex Freund explained it. Otherwise, I think it is not possible to "activate" "Calculate Feeds and Speeds" in the MKE.

 

 

Salvador Peregrina
Systems Engineer | NX 11.0.2.7

Re: Automatic updated Feeds and Speeds

Valued Contributor
Valued Contributor

Hi,

 

I have defined constants in MKE. Those I am assingning to the Feeds and speeds operation-functions.

I have tried, and yes it is not working :/

NX 11.0.1.11

Learn online





Solution Information