Cancel
Showing results for 
Search instead for 
Did you mean: 

Back Bore Milling Operation

Creator
Creator

Is it possible in NX10 to mill/interpolate a back bore feature using a slot milling tool?

11 REPLIES 11

Re: Back Bore Milling Operation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Short answer: As long a sthe tool fits down the hole, yes.

 

Multiple ways to do it, I'd try planar mill.

Use avoidance geometry (start/return points) and engage/retract as needed.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Back Bore Milling Operation

Creator
Creator

Thanks for the input. I was able to get it done by using Planar Profile and setting the floor distance to the width of my grooving tool.

Re: Back Bore Milling Operation

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

There is no dedicated operation for this yet. Radial groove milling comes the closeset but it currently requires a bottom.

If it's just a single cut level use planar profile with a tracking point on top of the t-cutter.

Re: Back Bore Milling Operation

Creator
Creator

Thanks. By using the Drive Point dropdown on Planar Profile, i can toggle between top and bottom tracking points of the groove cutter. Very cool

 

Re: Back Bore Milling Operation

Legend
Legend
If possible, would you share an example?
Highlighted

Re: Back Bore Milling Operation

Experimenter
Experimenter

You can do it using Generic Motion operation in this case you will have better control on your toolpath.

Generic Motion.jpg

TC10 NX9 + BCT16 Platform

Re: Back Bore Milling Operation

Creator
Creator

Re: Back Bore Milling Operation

Creator
Creator

I'm not familiar with the Generic Motion operation. How do you access this operation?

Re: Back Bore Milling Operation


@Lynn_B wrote:

I'm not familiar with the Generic Motion operation. How do you access this operation?



Generic Motion is found in the mill_multi-axis and probing template types.

gmc_tooltip.jpg

Mark Rief
Retired Siemens

Learn online





Solution Information