Cancel
Showing results for 
Search instead for 
Did you mean: 

Bad track post-processing in Postbuilder

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,
I have a postprocessing problem with a two-channel lathe. When I make turning operations and then milling and drilling, and when I generate all the operations of one channel, turning operations are fine and milling and drilling have pointless coordinates and some features are missing. When I only generate milling and drilling operations, that's all they have to be. Would anyone not know what to do? I also have reset everything on the bottom of each operation, but it did not help.

Thank you

 

SAMOSTATNE_VRTANI.PNG

1 REPLY 1

Re: Bad track post-processing in Postbuilder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

1) Do you have linked posts (one for turning, one for live tooling)?

1A) if so, how do you switch posts? (the usual way is using "Method" view parents, with the "HEAD" UDE attached as a start event on the method)

1Ai) if above is true, is *every* operation under the correct method view parent (rather than under the top level "METHOD")

 

If not, how are you switching between kinematics/posts?

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information