Cancel
Showing results for 
Search instead for 
Did you mean: 

Ball Nose Tip Compensation in Nx

Valued Contributor
Valued Contributor

Hi All

I am searching for the tip compensation of Ball Nose in NX cam but unable to find it.

In Mastercam this option exists but in Nx Cam i don't Know.

If any one knows about this option in Nx cam, please share me where i can get this....thanks

 

A screen shot from mastercam is attached here just for illustration purpose.

Mastercam Tip Compensation.JPG

4 REPLIES

Re: Ball Nose Tip Compensation in Nx

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if you mean output for center of Ball Nose, it can be done by customizing you postprocessor.

There is PB Command which you can import to you postprocessor

 

    #=============================================================
    proc PB_CMD_center_of_ball_output { } {
    #=============================================================
    #
    #  This command will output center of ball in every linear,
    #  circular and rapid move block.
    #
    #  This function is only valid for the Fixed and Variable Axis
    #  Surfacing Contouring modules in NX2 or newer.
    #
    #  You will also need to toggle on the Output Contact Data option
    #  on the Machine Control or Non-Cutting Moves (More tab) dialog.
    #
    #
    #  ==> Import this command to the post and call it in the
    #      PB_CMD_before_motion command.

 

But there is also 3D cutter compensation (inside NX). I'm not sure which option you are referring to.

2017-12-12_16-36-20.jpg

 

Marek Pawlus, NCmatic

Production: NX 12.0.1
Development: C#, Tcl/Tk, CSE

Re: Ball Nose Tip Compensation in Nx

Valued Contributor
Valued Contributor

@Marek_Pawlus

I am using HeidenHain Post processor  which perfectally generating codes for TCPM or M128.

which is used for Axis Synchronisation and 3D cutter compensation.

I mean there is not any issue in my post processor.

I just want to know where the option" 3D cutter Compensation" is inside NX cam.

 

Thanks for reply

Re: Ball Nose Tip Compensation in Nx

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

About postprocessor I didn't mean that it needs to be fixed. I mean that there is an option to add a FEATURE, which allows you to output code for center of the ball.

 

And 3D cutter compensation can be found Non Cutting Moves / More tab / Output Contact Data

2017-12-12_17-05-25.jpg

 

 

This two options are not related to each other.

Marek Pawlus, NCmatic

Production: NX 12.0.1
Development: C#, Tcl/Tk, CSE

Re: Ball Nose Tip Compensation in Nx

Valued Contributor
Valued Contributor

@Marek_Pawlus

Thank you for your kind help.

This is exactly i was searching for.

Learn online





Solution Information