Cancel
Showing results for 
Search instead for 
Did you mean: 

Best practice to machine NPT inner threads in NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Usually we are only used to machine metric threads, but now we also have to machine NPT threads.

How do you machine NPT inner threads with NX currently?

What are the do's and don't's?

 

More or less a best practice guide for machining NPT inner threads with NX, with the option to do this through FBM, which we are heavily using.

 

NX is designing the geometry of a simplified NPT thread with a cylindrical face, but the face is conical in reality, so that is another hurdle to get over.

 

Thanks in advance for any pointers for a metric thread user Smiley Wink

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
2 REPLIES

Re: Best practice to machine NPT inner threads in NX

Gears Legend Gears Legend
Gears Legend

If the thread is modelled with NX as Threaded hole with NPT thread, the simplified representation is a cylindrical face, but when you do a thread milling operation you will see a conical helix.

NPT threadmilling.png

Patrick Delisse
KMWE - DutchAero
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: Best practice to machine NPT inner threads in NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks for pointing this out, we haven't tried yet how this works in NX 10, since we are currently migrating to it.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information