Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Bring in assembly defined tool native library

I'm trying to get a tool in from the native NX tool library which is an assembly. If I try to import it in I get the following error. However if I bring in a sample NX tool that's an assembly and then my tool comes in fine. It's like there is something I didn't define in my part file that is in the NX one, but I can't figure out what it is.

 
 



&MACRO DIALOG_BEGIN "Search Result" 0 ! DA2

&MACRO BEG_ITEM 9 (1 BOOL 0) = 0 ! Preview

&MACRO CUSTOM 25 EASYTL * TL_SELECT * (4) * 0 * 1 ! TOOL-62_A88

&MACRO CUSTOM 25 EASYTL * TL_DEFAULT_ACTION * (4) * 0 ! TOOL-62_A88

&MACRO END_ITEM 9 (1 BOOL 0) = 0 ! Preview

&MACRO DIALOG_END 4, -1 ! Search Result: mtEndEventLoop

&MACRO FOCUS CHANGE IN 1



NX Load Options Are :-

Load Options : Load as saved

Load Latest : Find exact version of partnames

Load Components : Load all the component parts

Failure Option : Do not abort load on failure

Load Fully : Do not fully load the component parts

Representations : Do not use lightweight

Load Substitution : Do not allow substitutions on load

Reference Sets : As Saved, None, Empty, Use Model

: Do not apply to all levels

Load Wave Data : Default load behaviour

Part family members : Regenerate missing members automatically

W:\Engineering\Programming\NX_CUSTOM\8.5\CAM\template_part\english\\library_dialogs.prt is on a ntfs filing system



Loading "W:\Engineering\Programming\NX_CUSTOM\8.5\CAM\template_part\english\\library_dialogs.prt" which was saved in NX V8.5

Read in all for part "W:\Engineering\Programming\NX_CUSTOM\8.5\CAM\template_part\english\\library_dialogs.prt", cpu 0.032, real 0.035

Partition info: RM:1 (0.0, 0.0) CM:1 (0.0, 0.0) EXP:1 (0.0, 0.0) PATT:1 (0.0, 0.0) OCC:1 (0.0, 0.0) KF:1 (0.0, 0.0)

Loaded and updated part "W:\Engineering\Programming\NX_CUSTOM\8.5\CAM\template_part\english\\library_dialogs.prt" cpu 0.032, real 0.042

*** EXCEPTION: INTERNAL ERROR in line 717 of O:\ugnx853\ip3\src\syss\error\ind\error.cxx at Wed Sep 10 13:11:36 2014 Pacific Daylight Time

+++ invalid parameter passed to system or STL function


Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Learn online





Solution Information