Cancel
Showing results for 
Search instead for 
Did you mean: 

Brush type deburring tools

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just wondering if there was any interest for the capability to define "brush" type deburring tools.  Example (first one Google returned that looked like our tools):

 

http://www.brushresearch.com/deburring-brush.php

 

I'm thinking the tool would need a max & min diameter, and also be set somehow to NOT remove material in verify/IS&V (I'm not sure how to model "deburring" material remove, if even desired - maye change color of facets that are "touched" by the tool?)

 

tool would go into any hole >= min diameter, but warn user if hole > max dia

 

Right now I'm defining as a 180° point drill.

 

Thoughts?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


1 REPLY 1

Re: Brush type deburring tools

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

We have been doing this in Vericut for years

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information