Cancel
Showing results for 
Search instead for 
Did you mean: 

C Axis Rotation For Drilling

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Polar.png  Does someone know how to drill this holes only rotate C axis?

3 REPLIES 3

Re: C Axis Rotation For Drilling

Legend
Legend

You should only see C rotations after the 1st hole if they are on the same axis.

 

Can you show your posted code?

Glenn Balon
Production: NX 12.0.2 MP7 Primarily CAM

Re: C Axis Rotation For Drilling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Assuming you have a 5 axis machine, you can use the "lock axis" UDE

I've never done it, but there have been posts in the past on this topic.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: C Axis Rotation For Drilling

Gears Phenom Gears Phenom
Gears Phenom

hi,

your tool path is 5 axis, straigth lines, but move is in 5 axis.

Consider if your machine have 5axis tranformations.

You can omit moves between holes somehow as well, but you can have problem in some other cases where is C rotating not enough.

It is pretty complex.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information