Cancel
Showing results for 
Search instead for 
Did you mean: 

CAM EAP 24 - Complex Milling

Siemens Phenom Siemens Phenom
Siemens Phenom

By the end of January, we expect to release CAM EAP 24 for evaluation and providing feedback to enhancements we are working on. In the Complex Milling area this EAP will expose many “goodies” we were working on recently. I want to provide a list of those with some high-level description. Those of you who are interested in one or more of these enhancements – please send me a mail with the following details: Company Name, Sold-to ID, contact person, main + sub Topic to evaluate. I will add you to the EAP customers list (if you are not part of it already) and per enhancement – will send materials better describing the functionality, workflow and known issues. if you do not have a valid NDA signed - you will need to sign it to get the EAP version and License.

Main Topic

Sub topics

evaluation Status

Details

5X Roughing

 

Initial

Multi-levels Roughing where the cut levels are offsets from arbitrary floor / ceiling or interpolation between the two. Cut pattern is follow part or adaptive with option for bottom up cutting. Support any tool type. Tool axis – perpendicular to the cut level

Multi-blade – blade finish

Swarfing - new alignment settings

Final

More control over the collision Handling– ‘Contact Top and Bottom’, ‘Degouge’ and ‘Balance’ stock. Also improved control to the extension Alignment

Guiding Curve

Barrel Mill support

Initial

Allow “Swarfing” with Tangent Barrel. User control for the ‘Swarf Angle’ and Ring Height (Default, Constant and Variable). Use Tilt Tool Axis (TTA) to smooth the path.

Taper Barrel tools are partially supported.

 

T-cutter

Final

Finish walls using T-cutter with full radius

 

Trim / extend

Initial

Control the coverage of a Guiding Curves operation with morphing pattern by trimming / extending the cut area. In some case you can combine those to get a flaring extension.

 

Interpolate along axis

Final

New Tool Axis option for axis-symmetric geometries allow the user to set various 4+1 angles relative to the rotary axis and Guiding Curves would interpolate the Tool axis in between.

 

Parametric interpolation

Initial

New tool axis option. To some extent like Interpolate Vector with ‘U’ or ‘V’ in Surface Contouring

 

Smart tool axis regenerate

Initial

Guiding Curves now allow to play with the Tool-Axis to optimize its behavior, and the regeneration is extremely quick (path / contact with the part would not regenerate).

The environment also allows you to analyze various aspects of the tool path without leaving the operation edit dialog.   

Usability

Flat dialogs (GC, Multi-Blade)

Initial

New templates using the Flat dialogs infrastructure to optimize the look and feel of these operations.  

 

Guided Workflow(?)

Initial

 

 

PoP in Op edit

Initial

From within the operation edit dialog you can now Pick on path to show the tool, play its animation, show with material removal, filter cut levels etc.

CAM Robotics

CSE Simulation – KUKA Robots

Initial

G-Code base Simulation (CSE) for robots using KUKA controller. Ability to work directly from NX or upload external program

 

Multiple Robots cell

Initial

Support cells with more than 1 robot working together to machine a part.

 

Yours,

 

Eddy Finaro
NX CAM Product Manager
Siemens PLM
6 REPLIES 6

Re: CAM EAP 24 - Complex Milling

Creator
Creator

Eddy_Finaro,

Hello,

 

Does 1847 include CAM EAP 24?

 

Yours,

wxy

Re: CAM EAP 24 - Complex Milling

Siemens Phenom Siemens Phenom
Siemens Phenom

No Wxy, 

 

NX 1847 development was closed a while back, while we progressed with the various developments. somo of the projects are embeded in 1847 and hidden behind ENV or missing templates, but for most the condition is inferior than the current state. are you interested in any in particular?

Yours,

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: CAM EAP 24 - Complex Milling

Creator
Creator
Eddy_Finaro,
I am interested in EAP 24, especially in 5X roughing on High speed milling, and is there an automatic avoidance function?

I think the automatic avoidance function in the 1847 version are very good, as well as the guide curve.

Yours,
wxy
Highlighted

Re: CAM EAP 24 - Complex Milling

Experimenter
Experimenter

Hello Eddy,

 

when the EAP 24 will start? We have some niche parts to test the 5X Roughing.

 

Thank you

Re: CAM EAP 24 - Complex Milling

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Nicolas and others,

 

The version and documentations are ready for a while, but some administrative and legel changes has to happen before you will get a mail with download and instalations instructions from GTAC.

The CAM EAP was renamed and it is called from now EVP - 'Early Validation Program'.

The ones registered to the program will get the lic file from GTAC and not from the product manager.

 

Nicolas - have you registered to the program already? 

 

Sorry for the delay. hope the version will become available soon.

 

Eddy

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: CAM EAP 24 - Complex Milling

Experimenter
Experimenter
Thanks Eddy. We got your Information about the EAP.

Just one more question where we get the template for the 5X roughing.

Thanks a lot for your help.

Learn online





Solution Information