Cancel
Showing results for 
Search instead for 
Did you mean: 

CAM Milling Vise

Legend
Legend

Up until recently I've been using fixed workholding *aka* Dovetail vises I made.

Now I'm using more Kurt and Self centering vises in my programming and like the jaws to be modeled as accurately as possible.

 

Right now I have some assemblies created with the vises. I import the vise into the CAM, wavelink the jaws, either custom model jaws or just position them correctly. It becomes a cluster managing everything.

 

What does everyone else do for this? Turn the vise into a "reuse"? Deal with wavelinks?

 


Dennis Rathi
Creations Unlimited
6 REPLIES 6

Re: CAM Milling Vise

Valued Contributor
Valued Contributor
I have fixtures as reusable parts. Jaw distance is made with a synchronous modeling dimension. When adding the part there is a short list with dimensions, but you can also type in width or diameter you want.
Easy to setup, explain and use.
W10 NX12.0.2.9
testing v1847

Re: CAM Milling Vise

I do the reuse library as well.  I leave the floating jaw with one degree of freedom and then override the position when I get it into my assembly.

Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Re: CAM Milling Vise

Legend
Legend
Are there any tutorials or instructions on how to convert it to a reuse part?

Dennis Rathi
Creations Unlimited

Re: CAM Milling Vise

Legend
Legend

Bump?


Dennis Rathi
Creations Unlimited

Re: CAM Milling Vise

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think there are some videos in the tech tips section of this board.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CAM Milling Vise

Community Manager Community Manager
Community Manager

Yes, there are a couple of nice Knowledge Base articles on using the Re-use Library:

 

Intro to using the Re-use Library by Mike Mannino

 

Library samples for you to download

Derek Hart
... if we're not having fun, we're not doing it right!

Learn online





Solution Information