Cancel
Showing results for 
Search instead for 
Did you mean: 

CAM Nx10 and Nx12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I have one problem. When I generate NC code in NX10 everythink is ok. But when I generate NC code in NX12 I get wrong output out (coordinats X,Y and Z are wrong). And PP is the same.

 

Can someone help me?

9 REPLIES

Re: CAM Nx10 and Nx12

Gears Phenom Gears Phenom
Gears Phenom

hi,

I get the same output:

 

firts tool apth point is:

GOTO/-66.2583,2.4257,318.3584,0.1218691,0.0002343,0.9925462

so 

34 L X-66.258 Y2.426 Z318.358 A-7. C270.11 FMAX  

 

But I see difference in your programs - first one is 5axis continual and second one is 3+2..

So difference in XYZ should by OK, but you should not to use rotary axes in this mode. (PLANE)

Anyway continuous 5ax tool paths is "dedicated" for such 5ax continous output. (M128)

So only thing what is wrong in your case is outputed 5axis mode Smiley Happy

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: CAM Nx10 and Nx12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Ok, thanks.

 

But I still not understant why I have M128 in NX10. And why I don´t have M128 in NX12.

The PP are the same.

What I need to fix in PP, to get M128 in NX12.

The operation is simultaniom (angle of the tool change many times).

NX10 I get good NC code., but with N12 I don´t good code.

But PP are the same.

Re: CAM Nx10 and Nx12

Gears Phenom Gears Phenom
Gears Phenom

I have M128 in NX10 and also in NX12.The same output.

Do you have some ude modes or something in use in one of the NX?

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: CAM Nx10 and Nx12

Legend
Legend

 

I've open your part and postprocessed with your post with both NX10 and NX12 obtaining identical output.

Cattura0.JPG

Are you sure you are referencing the same post in NX10 and NX12 configuration? ( for example NX12 template_post.dat could reference a different event handler)

try to put the post in an empty folder and then browse for post both in NX10 and NX12 to exclude that the problem is from configuration

Cattura.JPG

Re: CAM Nx10 and Nx12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I put PP in empty folder but still doesn˙t work.

But I still get different output.

Re: CAM Nx10 and Nx12

Legend
Legend

wich version of NX12 are you using?

I'm on NX 12.0.1.7 MP1, 29Apr18.

Re: CAM Nx10 and Nx12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

my version is NX 12.0.0.27 MP1 08Dec17

 

Maybe is that the reason.

I will download the updates.

Re: CAM Nx10 and Nx12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Yes now works ok!

Thanks a lot Ibonomi.

 

 

Re: CAM Nx10 and Nx12

Legend
Legend

glad to hear that

ciao

Learn online





Solution Information