11-02-2017 09:00 AM
Solved! Go to Solution.
11-02-2017 11:31 AM
From what I can see...(it's a bit hard from you picture to figure out if this is what's going on)
1) Geometry view needs 3 sets of MCS/Workpiece/turning workpiece setups
- left spindle
- cutoff position
- right spindle
2) In "turn workpiece" objects for 2nd/3rd "setups", in specify blank, select "Workspace" option & From & to positions
- center - curve to select are left & center part positions
- right - curves are center & right part positions
3) Make sure to "transfer" the workpiece only ONCE
i.e. first operations only use "left" setup
then operations only use "cutoff" setup
then operations only use "right" setup.
If you go back & forth (left-cutoff-left-cutoff-right-cutoff) the IPW gets transferred more than once, and goes off in space.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled
11-03-2017 02:56 AM