Cancel
Showing results for 
Search instead for 
Did you mean: 

CAM linked geometry, holemaking

Phenom
Phenom

Since CAM started creating automatic linked geometry we have created a linked body in our cam files to minimise the random feature creation. also this helps with creating check, drive, tool axis and other geometry if required.

 

Holemaking seems to creates some issues, I am not sure if these are related to selecting geometry from the linked body rather than the component.

 

Create holemilling geometry and operations, then move the component the linked body updates but the holemilling geometry stays in the original location.

 

Deleted the CAM setup, start a new CAM session and the hole making geometry is still fubar!!

 

Is the underlying holemaking geometry not part of the CAM setup? How can we clean this up?

 

What is the best practice for:

  1. Dealing with the linked geometry situation?
  2. Selection of CAM geometry from linked bodies or components?
  3. Selection of holemilling geometry?

Alex

NX9.0.3.4 mp5

Win7 Pro

 

4 REPLIES

Re: CAM linked geometry, holemaking

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The new drilling operations introduced in NX 9 use FBM machining features, so you will have to check them out in the machining feature navigator in CAM.

There you can approve any changes applied to the feature, so that they get inherited by the operation.

 

We are always using linked bodies and haven't had any problems that the hole geometry didn't update the hole position.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CAM linked geometry, holemaking

Siemens Phenom Siemens Phenom
Siemens Phenom

Hole milling on linked bodies isn't working any different from hole milling on "regular" NX geometry. The hole milling geometry automatically updates to the new location (I just tried it).

 

Please share a copy of your problem part if it doesn't work for you.

 

Tom van 't Erve

NX CAM Development

Re: CAM linked geometry, holemaking

Phenom
Phenom

This may be related to some other problems with parasolid imports.

 

I found another issue yesterday were selecting hole geometry from an imported solid works parasolid would freeze the display. Luckily this is already fixed in mp6.

 

Any idea on why deleting cam setup doesn't clean up FBM objects?

 

 

MP6 7321100 Graphic window freezes when a Find Feature is run to Parasolid model.

MP6 7321742 Graphics window freezes after parametric feature recognition of SE part

MP6 7323594 NX CAM graphics lock when Hole or Boss geom group -Solid Edge generated part.

Re: CAM linked geometry, holemaking

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@agrivas wrote:
Any idea on why deleting cam setup doesn't clean up FBM objects?

 

The setup is only affecting the ONT, machining features are not part of how the part is placed on the machine or how it is machined.

The machining features are not bound to the machine, they are general objects valid for any machine.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information