Cancel
Showing results for 
Search instead for 
Did you mean: 

CAM materials and CAD materials

Gears Phenom Gears Phenom
Gears Phenom

In NX9, are the materials linked yet?  ie, if I assign a material in CAD (Tools, Assign Material), will this translate to the CAM side, or do they have to assign the material also?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
4 REPLIES

Re: CAM materials and CAD materials

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This not not even implemented in NX 11.

Create an enhancement request at GTAC for this functionality, so that there is a higher priority assigned to this request.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CAM materials and CAD materials

Gears Phenom Gears Phenom
Gears Phenom

ER is in process, I'll share the number once it's in the system.  I think I submitted an ER for this back in NX5 too

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: CAM materials and CAD materials

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Currently NX uses a separate material library in each of the following modules:

  1. modeling
  2. simulation (FEM, CAE, etc.)
  3. tooling design (Mold, Die and Progressive Wizards)
  4. manufacturing
  5. high quality rendering

I think these are just a small excerpt and that there are even more.

Would be nice to have one material library with all the information need, so that the material specified during the design of a solid can be utilized in each of the subsequent modules of NX.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CAM materials and CAD materials

Gears Phenom Gears Phenom
Gears Phenom

ER 7802931

 

Please add yourselves, to get it some weight.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Learn online





Solution Information