Cancel
Showing results for 
Search instead for 
Did you mean: 

CAN'T Remove all Material at the ID in TURNING

Pioneer
Pioneer

I'm trying to clean off the ID in Turning, but I don't know why there 's still some material left in the radius, the insert doesn't want to reach. 

 

1. Using the Round Insert with Contour Cutting

 photo Untitled_zpsxrbkljqv.jpg

 

2. Using 80 degree Bore ID with Linear Cutting

 photo 80degree_zpsrocpsncn.png

 

I've tried many operations to remove the Red Circle Area, but they all excluded this area.

Please help me how to overcome this issue.

 

Hoang

 

2 REPLIES

Re: (Turning) Round Insert with Contour Zig Cutting Question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Do you have different face & radial stock?

Cutting params button, I forget which tab.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: (Turning) Round Insert with Contour Zig Cutting Question

Pioneer
Pioneer
Ken_A,

No, I don't, I keep face & radial stock equally, you can see all the other radial stock already cleaned up after roughing, and only the red circle area is remaining.

I tried to use 80degree insert ID bar to clean that area, it happened the same, it didn't want to machine the red circle area.

Learn online





Solution Information