Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

CIRCLE output in CLS

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

The default output of a full circular motion in STANDARD_CLSF is 3 CIRCLE records of each 120 degree arcspan

Is this a way to change this?

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET
2 REPLIES 2

Re: CIRCLE output in CLS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX internally calculates circles in 120° segments, so you would need to add some logic to the CLSF processor to change this.

On the other hand, why would you like to change this?

In this case, on a Heidenhain controller, you would never get a "invalid circle end point" error, with look ahead there would never be any circle pieces skipped, etc.

You would get the most accurate circular records possible if you just use what the system calculates internally.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CIRCLE output in CLS

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

It's not somethig I want to change, I was just wondering IF it could be infleunced.

In our postprocessors (Icam) we can set limits to the max arc-span of a circle, witch we don't use because of the 120 degree limit NX uses to output circles.

 

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Learn online





Solution Information