Cancel
Showing results for 
Search instead for 
Did you mean: 

COMBINE ROTARY HELP

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I use this cool thing but I have two questions abut this commands:

 

1. Is there possibility to avoid splitting bigger rotations to strange numbers?

(full circle with rotating A)

24 L A+0 FMAX 
.
34 L Y+3.721 Z+24.195
35 L Y+2.538 Z+23.669
36 L Y+1.288 Z+23.335
37 L Y+0 Z+23.2
*38 L A-177.062 why these values?
*39 L A-353.974
40 L A-360
41 L Y-1.288 Z+23.335 FQ107
42 L Y-2.538 Z+23.669
.

2. Is there any sense to have some extra values outputed?

Drilling 4 holes/ by 90deg:

19 L A+0 FMAX 
20 L X+30 Y+0 R0 FMAX M3
21 L Z+350 FMAX
22 L X+30 Y+0 R0 FMAX
23 CYCL CALL
24 L Z+350 A+1.5 FMAX ??
25 L A+90 FMAX
26 L X+30 Y+0 R0 FMAX
27 CYCL CALL
28 L Z+350 A+91.5 FMAX ??
29 L A+180 FMAX
30 L X+30 Y+0 R0 FMAX
31 CYCL CALL
32 L Z+350 A+181.5 FMAX ??
33 L A+270 FMAX
34 L X+30 Y+0 R0 FMAX
35 CYCL CALL
36 L Z+590 FMAX M92
37 L X+900 Y+601 FMAX M92
38 M30

 

Thank you for your help or explanations

 

jb

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
8 REPLIES 8

Re: COMBINE ROTARY HELP

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Juraj

If you shared your post and sample part we can help you understand why you are getting the results.

Regards

Paul

Re: COMBINE ROTARY HELP

Legend
Legend

Hi,
To avoid extra values in rotations, use the procedures from custom library of Postbuilder.
See them in pb_cmd_combine_rotary.tcl.

Re: COMBINE ROTARY HELP

Gears Phenom Gears Phenom
Gears Phenom

@Paul_Hartrick

see attachment

in drill there is some extra A:

%
.
N0040 G00 G90 X5. Y0.0 A0.0 S0 M03
N0050 G43 Z35. H00
N0060 G81 X5. Y0.0 Z8.599 R15.5 F250.
N0070 G80
N0080 G00 A-4.737 ***
N0090 A-90.
N0100 G81 X5. Y0.0 Z8.599 R15.5
.

milling looks better:

N0040 G00 G90 X0.0 Y1.44 A-180. S0 M03
.
N0080 Y.569 Z12.637
N0090 Y0.0 Z12.5
N0100 A0.0
N0110 A180.
N0120 Y-.569 Z12.637
N0130 Y-1.043 Z12.981

in other postprocessors it is worse, I dont know n what it depends

@FROBI

this behaviour is with combine rotary

 

thanks

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: COMBINE ROTARY HELP

Legend
Legend

See your toolpath and the cycle with extra move GOTO (why???):

toolpath.jpg

So you have

G00 A-4.737

As for milling, the lines are good, according the logic of the procedure PB_CMD__combine_rotary_check. The rotary combination is limited by 180 degrees there. So you have A-180, A0, A180.
If you want to move from -180 to 180 at once, modify this logic.

Re: COMBINE ROTARY HELP

Gears Phenom Gears Phenom
Gears Phenom

try test the same operations, or just variable contour,  by this another PP in attachment

there is no 180 deg logic :

N0040 A-180.
N0050 G00 G90 X0.0 Y1.44 S0 M03
N0060 G43 Z14.058 H00
N0070 G01 Y1.348 Z13.48 F250. M08
N0080 Y1.043 Z12.981
N0090 Y.569 Z12.637
N0100 Y0.0 Z12.5
N0110 A-355.5
N0120 A-531.
N0130 A-540.
N0140 Y-.569 Z12.637
N0150 Y-1.043 Z12.981
N0160 Y-1.348 Z13.48
N0170 Y-1.44 Z14.058
N0180 M02
%

 

 

 

I dont understand this you wrote, in drilling:

goto 5,0,12.5 caused this:

G00 A-4.737

?

Could you please clearify it better to me?

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: COMBINE ROTARY HELP

Legend
Legend

Have you looked into the source of the the procedure PB_CMD__combine_rotary_check?
There is the flag mom_sys_skip_move here with values YES or NO. The extra moves are added when it is NO.
The conditions of skipping depend on comparizon of mom_prev_pos and mom_pos.

After your cycle of drilling: Zprevious=12.5 is not equal Zcurrent=35., so flag of skipping is NO, and then output G0 A-4.737. For milling another condition works here, comparing current angle with last_4th_output.

Re: COMBINE ROTARY HELP

Gears Phenom Gears Phenom
Gears Phenom

Nice, thank you! I dont realized there is Z in the cycle in variables Smiley Happy

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: COMBINE ROTARY HELP

Experimenter
Experimenter

Hi brother
How do you solve the problem, I have no effect after adding it, thank you

Learn online





Solution Information