Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE: 4th head in standard machine Sim16

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi all!

I want to add 4th head to  standard machine Sim16.

Head N4 is the same as standard head N1.

I attached the standard postprocessor and CSE (BUT!! - I added output of number of 4th head to command "HEADCHANGE" in that postprocessor and I edited subprogram "HeadChange.SPF" in CSE-folder).

 

But I have mistake (see photo "222").

What I did wrong?

Thanks very much!

 

 

 

 

6 REPLIES

Re: CSE: 4th head in standard machine Sim16

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Alexis,

 

I think you have to rename the tool in the ONT to an ending "xxx_4" as the command two lines above is looking for:

 

sToolName = getArrayElement("$TC_TP2",nToolID)+"_"+getVariable("$P_HEADNO");

 

Kind regards

 

Gregor

Re: CSE: 4th head in standard machine Sim16

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hi!
I did
sToolName = getArrayElement("$TC_TP2",nToolID)+"_4");

And it did the same bad result as above((

Re: CSE: 4th head in standard machine Sim16

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Please do not edit the command, but the name of the tool in the NX-Machine Tool View from "UGT0202" ==> "UGT0202_4"

In the document "D:\Siemens\NX10\MACH\samples\nc_simulation_samples\Working_with_OOTB_MACH_Simulation_Examples.pdf in chapter 13 is described the background of that issue.

Kinde regards

Gregor

Re: CSE: 4th head in standard machine Sim16

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thanks!
It is work! I edited tolname to "MILL_4" and it started working
But it is strange! - Heads 1-2-3 work without additional renaming of the tool installed in them: "MILL" for example

Re: CSE: 4th head in standard machine Sim16

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Oh, I'm sorry, I saw!
Thank you for explaining! I saw:
In other channels in basic example:
UGT0202_001_2
UGT0202_001_3
You're right! All right! Thank you! I could not solve this riddle half a day!

Re: CSE: 4th head in standard machine Sim16

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

For those who have not understood yet, the picture:heads.png

Learn online





Solution Information