Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - CTRANS / UIFR

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everybody,

 

I develop a 5 axes machine in NX9 with the axes X1, Y1, Z1, B1 and C1.

Now I want to do a zero fixture offset with CTRANS or UIFR like :

 

CTRANS(X,-23.332860808555,Y,0.19077622194288,Z,5.133,C,22.5)

 

So I get an error, that a frame could not be created. I set C to C1 and it works.

But in which method the frames are created?

 

Ok, mostly the axes named as C or B and so it works.

 

Best wishes from Hamburg

Viktor

4 REPLIES

Re: CSE - CTRANS / UIFR

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi VikP,

For any axes the system looks at the channel axis names and afterwards to the machine axis names. When this is ok then a frame will be created. X, Y, Z are mapped automatically to the GeoAxes.

Thomas

Re: CSE - CTRANS / UIFR

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Thomas,

 

ok, thanks.

Is it possible to manipulate the check in the cse drivers?


Viktor

Re: CSE - CTRANS / UIFR

Siemens Phenom Siemens Phenom
Siemens Phenom
Write your own CTRANS in MCF/CCF ;-)

Re: CSE - CTRANS / UIFR

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Mh, ok Smiley Happy

Learn online





Solution Information