Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

CSE - CYCL DEF 301 solution

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

has anyone a solution to use CYCL DEF 301 with CSE simulation?

 

 

Thanks and best wishes from Hamburg

 

VIktor

6 REPLIES 6

Re: CSE - CYCL DEF 301 solution

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Best regards from Moscow!

I open Cycle programming manual for Heid530, and, excuse me, I cannot find CYCL DEF 301.

ITNC OR PILOT? Can you send short description?

Re: CSE - CYCL DEF 301 solution

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I have unfortunately no further information.

 

This cycle is similar to the PLANE SPATIAL and is made for MATEC tool machines.

Re: CSE - CYCL DEF 301 solution

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Any CYCLE that is created by the machine tool vendor needs to be implemented manually.

 

The easiest is to call an external "Any-Controller" program as it is done with the tool change, this would then call the correct PLANE SPATIAL block.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CSE - CYCL DEF 301 solution

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thank you all!

 

For the first, I use the PLANE SPATIAL for the simulation.

Re: CSE - CYCL DEF 301 solution

Siemens Creator Siemens Creator
Siemens Creator
Hello VIktor

For the post processor, how did you applied the CYCLE DEF 300? As a UDE or as part of the rotation definition?

Thanks and best regards from Mexico!

Re: CSE - CYCL DEF 301 solution

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello PabloMF,

 

in my postprocessor this cycle is used for every swiveling operation and defines the rotation, so I don't need an UDE for the output.

 

Best wishes

Viktor

Learn online





Solution Information