09-04-2015 03:43 AM
Hello,
has anyone a solution to use CYCL DEF 301 with CSE simulation?
Thanks and best wishes from Hamburg
VIktor
Solved! Go to Solution.
09-05-2015 04:03 AM
Best regards from Moscow!
I open Cycle programming manual for Heid530, and, excuse me, I cannot find CYCL DEF 301.
ITNC OR PILOT? Can you send short description?
09-09-2015 09:06 AM
I have unfortunately no further information.
This cycle is similar to the PLANE SPATIAL and is made for MATEC tool machines.
09-10-2015 10:25 AM
Any CYCLE that is created by the machine tool vendor needs to be implemented manually.
The easiest is to call an external "Any-Controller" program as it is done with the tool change, this would then call the correct PLANE SPATIAL block.
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0
Employees of the customers, together we are strong
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
09-10-2015 12:03 PM
Thank you all!
For the first, I use the PLANE SPATIAL for the simulation.
12-15-2016 05:45 PM
12-16-2016 01:43 AM
Hello PabloMF,
in my postprocessor this cycle is used for every swiveling operation and defines the rotation, so I don't need an UDE for the output.
Best wishes
Viktor