Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - CYCLE800 + Head-Chain - NX 11.02. MP5

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

currently I'm working on a 5-axis millturn machine with a head modul. (DMC 125FD mB - B/C kinematic)

We use CYCLE800 for programmed swiveling planes.

 

The CYCLE800 uses both kinematics, machine + head. In CSE it works fine.

 

BUT, there is one head option which makes many problems.

If I just want to position at 0/0/0 the machine axes get inverse to UIFR.

 

I don't get it. Look at the picture, please.

 

2018-02-01 22_15_12-ConmatiX - NX CAM 11 SHARE - Fertigung - [SKF_180125_125FD_CAM.prt (Geändert) ].png

 

Regards, Viktor

2 REPLIES

Re: CSE - CYCLE800 + Head-Chain - NX 11.02. MP5

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Please check the soft limits of your lathe spindle Smiley Happy

 

Unlimited limits were wrong in this case.

 

 

Re: CSE - CYCLE800 + Head-Chain - NX 11.02. MP5

Experimenter
Experimenter

CSE needs to be adjusted via whatever parameter TC or UC---  this meaning ---  your simulator is not correct (INI file) and stating such is incorrect ~~  esp for a Ledend..  lol   no woriies..  learn your control and the particular kinematics to adjust in you CSE subfolder to show the correct - simulation movement -- thus indicating your true movement in the real world and you answer should be apparent ...   always have the sim show the real world because then you can reverse the improper data input you selected for the swivel solution....  

Learn online





Solution Information