Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE ERROR: The programed target point is not in the circle path.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello there,

 

I have changed the postprocessor variable:  "mom_kin_machine_resolution"  from 0.001 to 0.01. 

 

And in MCF file I have Variable "Motion precission" = 0.01. 

 

But i get the next error in simulation (Image attached). 

 

This error begin when I changed "mom_kin_machine_resolution", never get it before. 

 

Any ideas?

 

Thanks,

Ivan

 

 

 

2 REPLIES

Re: CSE ERROR: The programed target point is not in the circle path.

Siemens Phenom Siemens Phenom
Siemens Phenom

Try to change the "Motion Precision" in the Machine Configuration. That value is related to the whole motion not to a single axis. The change inside the Post Configurator is related to each single output X, Y,Z etc. As you see the deviation is 0.11 (1.944 vs. 1.944) and so larger than 0.01 Motion Precision in MC.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE ERROR: The programed target point is not in the circle path.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi!

 

Thak´s for all. 

 

That resolve my issue. 

 

Best regards

Ivan

Learn online





Solution Information