Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE Heidenhain M128 command error

Valued Contributor
Valued Contributor

Hello

 

Im putting up new machine simulation based on Sim_08 heidenhain.

I made copy of directory changed 3D model and made new machine tool model.

I named kinematic chain to same as orginal sim_08 "Z-X-Y-A-C".

 

Everything else works correctly, but M128 command gives error:

Specified Kinematics chain default does not exist

Command  'SetKinematicTransformation' called with invalid argument

unspesified error .... GMe_Set5axisTransformation.

 

Any idea What is causing this?

Plane and Cycle_19 commands works just M128 gives error. 

 

 

4 REPLIES

Re: CSE Heidenhain M128 command error

Siemens Phenom Siemens Phenom
Siemens Phenom

NX Version?

Re: CSE Heidenhain M128 command error

Valued Contributor
Valued Contributor
NX10.0.3
Original sim08 works.
But copy and remade machine tool model won't.

Re: CSE Heidenhain M128 command error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Jussi,

 

either you rename the chain in kinematic model to "default" or you create M128 in MCF file like this.

 

2017-02-13 15_23_16-Machine Configurator - [G__kit_mach_resource_library_machine_installed_machines_.jpg

The problem is that (for any reasons) the M128 in CCF file do not transfer the strChainname to the method. In this case "default" will be used. 

 

This is fixed in NX11.

 

Thomas

Re: CSE Heidenhain M128 command error

Valued Contributor
Valued Contributor

Hello

 

Works like a charm.

Thanks

Learn online





Solution Information