Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: CSE. Machine with three channels. Management of synchronization labels

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

SetSyncPoint is a CSE kernel command to be used in any Meta code or method it is not needed to change the python parser to use these functions.

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE. Machine with three channels. Management of synchronization labels

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you Thomas! Excuse my obsession!
However, I need to solve the problem, the deadlines are very limited. How can I apply this "SetSyncPoint" procedure, only one example?

 

upper turret                  lower turret                   subspindle

L100                          L100                          L100    

...........................

L200                          L200                          L200 

...........................   

L300                          L300                          L300    

 

I found a similar procedure in Sim15 Siemens. And tried to apply it. But I had problems with the WAITM Command (see above). Can you give an example of "SetSyncPoint" procedure for Fanuc, which will synchronize 3 channels (similar to the WAITM command in Sim15 Siemens)

Re: CSE. Machine with three channels. Management of synchronization labels

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Alex,

 

see the following purely ficitonal sample how to syncronize motions on a 3 channel machine with the SetSyncPoint cse command

 

2017-11-03 10_11_15-SyncMotions_Sample.pdf ‎- Microsoft Edge.pngNC Code sample2017-11-03 10_10_59-SyncMotions_Sample.pdf ‎- Microsoft Edge.pngCSE Implementation

Re: CSE. Machine with three channels. Management of synchronization labels

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thomas, that's great! Your technique worked! Very grateful!

Re: CSE. Machine with three channels. Management of synchronization labels

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
Hi guys,

I have the same problem in my 3ch mkits with 3 turret.

Can you explain how use this CSE Implementation?

Learn online





Solution Information