Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - Message "Error in inverse kinematics solver"

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

while simulating a 840D nc code witt NX9 I get the following message:

--> "Error in inverse kinematics solver"

 

The code looks like:

--> "N0449 X-412.67970 Y74.11190 Z100.08660 A3=-0.70162 B3=-0.12119 C3=0.70217"

 

How can I delete these message? Does someone knows this alarm?

Best wishes from Hamburg,


Viktor

 

3 REPLIES

Re: CSE - Message "Error in inverse kinematics solver"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi VikP,

 

I know this alarm and you can´t delete it easily ;-)

 

This message comes up when the IKS can´t solve the calculation for the inverse kinemaitc due to the input (target) vector. Reasons for that can be a wrong vector or the machine kinematic is not able to move to this angles.

 

You can try to change the axis limits in kinematic model or MCF (I don´t know where the limits come fromin your project) that the IKS calculates another solution which can be reached from the axis.

 

Thomas

Re: CSE - Message "Error in inverse kinematics solver"

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Victor,

 

are you sure that the  kinematics - plus its axis limits - can reach the programmed position?
That looks like TRAORI in axis mode.

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE - Message "Error in inverse kinematics solver"

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

thanks for the fast feedback.

 

I already noticed that the axis limit is violated and so the alarm appears.

Ok, this problem is solved.

 

Thank you!

 

Best wishes

Viktor

Learn online





Solution Information