Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE OPSTOP and Block Skip

Phenom
Phenom

Using CSE with machine code is it possible to set OPStop to valid and set block skips.

 

 

Sometime I would like the CSE to stop at the M01 we have at each toolchange

This allows me to check the IPW state before continuing to the next operation.

 

Also we use block skip (1 thru 9) for other processes and it would be nice to enable and disable individual opskip's

 

If this is possible I cannot find it, otherwise it is probably an ER

 

Thanks

 

Alex

NX 9.0.3.4 MP15 (Production)

NX 10 11 12 (Testing)

2 REPLIES 2

Re: CSE OPSTOP and Block Skip

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Dear Agrivas,

to stop simulation at each operation change in CSE, you can define a "Matching Breakpoint" (available since NX11). For this type of breakpoint, you can define a string (e.g. "operation" or "M6") and simulation will stop at each NC Code lines which contains this string.

Regarding the skip levels, this is somethine we introduced in NX 12.0.1. (You can find them in the "Advanced" Area of the Simulaltion Settings).

Hope this helps.

Best regards.

Claus 

NX CAM Product Manager

Re: CSE OPSTOP and Block Skip

Phenom
Phenom

@ClausMichelfeit Thanks I will check it out

Learn online





Solution Information