Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE Okuma with GV_bUseLoadOffset FALSE

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

 

I´m doing a CSE simulation and there is something isn´t working fine.

 

I have a global variable GV_bUseLoadOffset with the value FALSE (In the code I put the values manually).

 

I think that the G15 H works OK, enter in the GME_ActivateOffset, and firstly dont use LoadOffset but at the end, It takes these values.

 

GV_False.JPG

 

GME_activate.JPG

 

In my code:

 

Fixture.JPG

 

At the end of GME_ActivateOffset..OK

 

final_GME.JPG

 

But finally...

 

Error.JPG

 

I don´t like Z-688 and CSE displaceOrigin this value..

 

Why does this happen?

 

Many thanks,

 

Best regards,

 

2 REPLIES 2

Re: CSE Okuma with GV_bUseLoadOffset FALSE

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Christian,

 

I shortly try to reproduce it with OOTB sim05 but failed. I mean I do not see the problem you seeing with that strange changing Z value. Please collect the data and provide it to GTAT for create an IR so that we could have a closer look into.

 

Thomas

 

Tested in NX10.0.3

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE Okuma with GV_bUseLoadOffset FALSE

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Christian,

 

as far as I understood your mentioned problem. If you want to switch between internal and external offset settings (LoadOffset True/False). You have to set the global variable "GV_bUseLoadOffset" TRUEor FALSE inside the "CSEInitializeChannel" method and not within the global variable settings.

 

ThomasF

Learn online





Solution Information