Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: CSE - PLANE SPATIAL with 45/45 degree Table

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Yes Thomas,

 

In my MCF file:

 

GV_strFourthAxisName  = "B"
GV_strFifthAxisName = "C"

Highlighted

Re: CSE - PLANE SPATIAL with 45/45 degree Table

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

If I push play I have this error:

 

00:00:00.00 Unspecified error when executing method 'getMainSpindle'.
00:00:00.00 Method getSpindleMode was called with an invalid argument type.
00:00:00.00 Command error! An if command couldn't be executed.
00:00:00.00 Unspecified error when executing method 'HandleTEvent'.

 

 

Re: CSE - PLANE SPATIAL with 45/45 degree Table

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

do you have a used main spindle in your kinematic model?

 

Best wishes

Viktor

Re: CSE - PLANE SPATIAL with 45/45 degree Table

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi Viktor,

 

I don't undestand what do you mean.

 

In my kinematic model there is only a spindle.

 

Emilio

 

 

 

Learn online





Solution Information