08-26-2015 07:06 AM - edited 08-26-2015 07:07 AM
Max diameter of part - 42 mm. Tool - D8. After milling:
Animation Accuracy: Fine.
Any advises - How I can get more better result?
NX 9.0.3.4
08-26-2015 07:26 AM
I have this in my environment file. I believe it allows for another setting called "extra fine"
set UGII_CAM_IPW_ENABLE_RGE=1
If that does't work try
# NX5 Preview Project - Facet Based IPW - Allows IPW Resolution-Extra Fine
UGII_CAM_IPW_ENABLE_RGE=“”
Hope it works for you.
08-26-2015 09:42 AM
What is the overall size of the part?
Is the accuracy mode needle count or tolerance? And what is the "fine" setting?
08-26-2015 09:50 AM
Dimension D26x15 mm.
Needle mode
Accuracy fine - Simulation Setting, Animation Accuracy
08-28-2015 03:43 AM
HEllo,
one more idea. Starting with NX903 settings for IPW and related tolerance are saved with the part file. Please check and change them to see if that solves the problem. You will wind them under:
Menu->Preferences->Manufacturing
Tab -> Geometry
Group -> In Process Workpiece Tolerances