Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - Preview Motion

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

I have an "interal error" if I want to open the "preview motion" option in the simulation assembly.

The machine was developed with NX 10.02., the customer uses this machine with NX10.0.0 and the following logfile entry appears:

 

*** EXCEPTION: INTERNAL ERROR in line 1921 of o:\ugnx100\ip24\src\part\no\ind\rm_entities.c at Mon Sep 07 10:00:36 2015 Mitteleuropäische Sommerzeit
+++ Class UGS:Smiley FrustratedvKim::KinematicChannel is not supplying an entity type for its objects.

 

Have somebody an idea what to do?

 

Thanks and best regards from Hamburg,

Viktor

2 REPLIES

Re: CSE - Preview Motion

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Viktor,

 

you must not use data with CAM saved and created in NX10.0.2 in NX10.0.

It sounds confusing, but we added new CAM features during the QRM releases, which makes it necessary to not use that in NX10.0.

 

For sure a internal error should not happens, but if you file a PR against it it will also not possible to fix it in the already released NX10.0. version.

 

You will find details information in the release notes of NX10.0.

 

 

 

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/release_notes/#uid:index_xid850184:xid862138:xid9...

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software
Highlighted

Re: CSE - Preview Motion

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

thank you very much.

 

An update to NX10.0.1 solved the problem and everything works now.

Learn online





Solution Information