Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE. Siemens 840D. How can I call the tool by tool number (T1, T2, etc)

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Now, CSE of Siemens 840D works with the type of tool invocation as:

N170 ;First Tool

N180 T="MILL_D30"    !!!!!!!!!!!!!!!!!!!!

N13 M6

N14 S300 M3

N15 G4 F5

N16 G54

N18 TRAFOOF

N20 G0 X-25.513 Y21.417 D1

N21 Z69.508

N22 M8

N23 G1 Z-109.742 F2000.

 

I have to do this format:

N12 T2 ; MILL_D30   !!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

N13 M6

N14 S300 M3

N15 G4 F5

N16 G54

N17 CYCLE832(0.02,112101)

N18 TRAFOOF

N20 G0 X-25.513 Y21.417 D1

N21 Z69.508

N22 M8

N23 G1 Z-109.742 F2000.

 

I fixed my postprocessor. But the CSE-simulator doesn't take a correction for the length (see attach figure).

How to fix it. Example of my machine is same "sim08_mill_5ax_sinumerik_mm"

2 REPLIES 2

Re: CSE. Siemens 840D. How can I call the tool by tool number (T1, T2, etc)

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
The question is lifted. Thanks to all!

Re: CSE. Siemens 840D. How can I call the tool by tool number (T1, T2, etc)

Experimenter
Experimenter

Hi, may we know how you fixed it? I have a simular situation. Maybe your solution could help me?

 

Thanks for sharing!

Learn online





Solution Information