Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE Simulation for CYCLE60

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello Guys,

 

you might help me: Is there any experience with the simulation of cycle60 (engraving) for sinumerik 840D controllers in a CSE simulation in NX CAM? If yes, is the implementation complex or do you just need to copy the cycle60 subprog in your cse_folder for your simulated machine?

 

 

Best regards

Simon

2 REPLIES 2

Re: CSE Simulation for CYCLE60

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you can get encrypted source file of this cycle (subprogram which you mentioned) it actually might work without much effort.
Otherwise you will have to create subprogram which will mimic real cycle behaviour, and this will need some more work.

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: CSE Simulation for CYCLE60

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Simon,

 

CYCLE60 is included in the SinumerikSL_Cycles_47_SP2_HF1.cyc file.

I´ve tested this cycle a few years ago with the older 4.4 cyc file and it works with the ootb sample machine.

 

I´m not sure if my test covers the real use case but there where no errors and the engraved text in the part.

 

Thomas

 

 

Learn online





Solution Information