Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - check for collision - NX12.01

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi everybody,

 

is it possible to activate the "Check for Collision" control for Tool/Part automatically? Customer Defaults?

 

2018-04-11 10_52_04-Simulation Settings.png

 

Regards, Viktor

6 REPLIES 6

Re: CSE - check for collision - NX12.01

Phenom
Phenom

Untitled.jpgMaybe this?

Re: CSE - check for collision - NX12.01

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Ji hjoy,

 

thanks for the fast feedback.

 

Unfortunately it does not work for machine simulation.

I think this check is just for the ISV simulation without machine.

Re: CSE - check for collision - NX12.01

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If it is not on the tab IS&V or IS&V options in the customer defaults, then there is no way to enable it by default through them.

Have you tried enabling it in the kinematic model of the machine? Select options from the context menu of the machine tool builder, when you pick an empty space, to get there.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: CSE - check for collision - NX12.01

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

With older NX versions the default way to enable collision check was the Machine-Tool-Builder in the kinematic part of the machine.

 

But no possibility with NX12, very strange. 

Re: CSE - check for collision - NX12.01

Legend
Legend

This is a bug. I also experienced this in 12.0.2 beta that I turned in as an IR. Hopefully they fix it.

 


Dennis Rathi
Creations Unlimited
Highlighted

Re: CSE - check for collision - NX12.01

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

thanks for bringing that to our attention, even better if we already have an IR.

We plan to fix it in NX12.0.2

 

Sorry for inconvenience

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information