Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - declaration of the variable has failed

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

I found a strange thing with NX 11.0.1.11 MP4 and Machine Configurator 1.0.0.1027 .

If a simulation is started and an error message appears for a failed variable declaration because of an accidental duplicated declaration, then I have to delete a declaration and HAVE TO quit the Machine Configurator for accept the change.

Otherwise the error message remains unchanged.

 

And is it right, that I have to reload a machine if a .cyc file is changed?

 

Regards, Viktor 

 

2 REPLIES

Re: CSE - declaration of the variable has failed

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Viktor,

 

"HAVE TO quit the Machine Configurator for accept the change."

Do you mean that you cannot press the save button in MC? 

 

The new cyc file content (same cyc file name ) will be used after "RESET"

 

Thomas

Re: CSE - declaration of the variable has failed

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

sorry for the late feedback.

 

The save button works. But sometimes I save and quit the Machine Configurator and no change was done.

And if I press the reset button, no changes. I reload the whole machine and changes are adopted.

 

I think it is a unique story.

 

Regards, Viktor

Learn online





Solution Information