Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - drilling and subprog _DEC1

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi everybody,

 

I've got an annoying error message.

The subprog "_DEC1" can't be found while the drill operation (CYCLE81/83 ...).

"_DEC1" is needed for the declaration of "_DMODE1", and then?

Does anybody have an idea for solution?

 

Perhaps the CSE driver are wrong.


Thanks and best wishes from Hamburg,

Viktor

2 REPLIES 2

Re: CSE - drilling and subprog _DEC1

Siemens Phenom Siemens Phenom
Siemens Phenom

You have to include the SMAC and PGUD Sinumerik defintion files to the 'MyMachine-CHANNEL.ini file. These two files are inside the cyc- package file and contain varaible declarations and definitions of sinumerik system variables, including the _DEC1 variables

 

When you use Sinumerik Cycles in NCK Version 4.5 or newer, you have to use the latest definition files.

 

ThomasF

Re: CSE - drilling and subprog _DEC1

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

so easy... but this Information about both "files" was missing.

Thank you very much!

 

Best wishes,

Viktor

Learn online





Solution Information