Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

CSE error - Kinematics Chain default does not exist

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello everyone,

 

I´m doing a simulation with a Personalised machine, with TNC control.

 

The 3 axis operations are correct.

 

But when I try to simulate an 5 axis operation I have a mistake with M128 and PLANE SPATIAL.

 

I found next error (image):

kineamtic_chain_default_not_exist.JPG

 

In Machine tool Navigator I have define a Kineamtic Chain --> Default. (Image)

 

machine_tool_navigator.JPG

 

 

 

Best Regards Ivan

3 REPLIES 3

Re: CSE error - Kinematics Chain default does not exist

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

  1. Make sure the „S“ Axis don’t have the “NC Axis” Flag checked
    and
    Don’t create any kinematic chain at all.
    A simple 5 axis machine tool the one possible chain will be found and used automatically
  2. Try „default“ in lower case
Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE error - Kinematics Chain default does not exist

Legend
Legend
"S" Axis should be defined as an Spindle and not as an Axis.
and as Tom sayed do not check the "NC Axis " Flag.

Heinrich

Re: CSE error - Kinematics Chain default does not exist

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi!

 

It works, thanks to both of you. 

 

Best regards

Ivan

Learn online





Solution Information