Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - high tool numbers

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

how can I solve the problem when a customer uses high tool numbers?

 

The tool parameters in the to_ini are declared as STRING.

The Metacode D is adjusted while the error message:
"Method getArrayElement what called with invalid argument to type"

 

 

 

2015-07-21 10_16_06-XML Notepad - C__Users_vpuzankov_Desktop_D_metacode.xml.png

 

3 REPLIES 3

Re: CSE - high tool numbers

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi

 

I'm pretty sure the 840D has a maximum tool number of 32000.

 

George

 

George Bennett
All NX versions
W7 Ultimate
Dell Precision M6700
Spirit of Innovation
Highlighted

Re: CSE - high tool numbers

Siemens Phenom Siemens Phenom
Siemens Phenom

George is right with the maximum of the array TC_DP[no] limit is 32000.

The problem is the data in the ini file need to be adjusted. Our OOTB post also has these limitation, but we suggest to not use bigger numbers.

 

On the controller the higher number might be the name like:

 

$TC_TP1[15]=521005
$TC_TP2[15]="UGT0201_088"
$TC_TP8[15]=10
....

 

What I say is the array has a limit


@Not-Yet-Retired wrote:

Hi

 

I'm pretty sure the 840D has a maximum tool number of 32000.

 

George

 



of 32000

 

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE - high tool numbers

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks for the great help and the advice.

 

I'll call the tools on the name and the problem is solved.

 

Thanks and good night!

Learn online





Solution Information