Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - multichannel simulation and single operatons

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

I use a multichannel turning machine in NX10.02. MP6. The simulation of single operations and the synchronize manager are working.

Now I need to try the simulation on NX10.03 MP1 and see there, I only can use the synchronize manager. If I want to simulate a single operation, the main_channel.ini files were not registered.
It seems like there is a changed sequence of loading the cse driver.

 

Do you now a problem like this?

 

Best wishes from Hamburg

Viktor

2 REPLIES 2

Re: CSE - multichannel simulation and single operatons

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

there is a known problem in NX10.0.3 when you select a single operation on channel two only and try to simulate (ISV) you get that message. Simulating a single operation on channel one should work. A PR call exists for this and development is fixing it.

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software
Highlighted

Re: CSE - multichannel simulation and single operatons

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Ok, thank you very much!

Learn online





Solution Information