Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - nurb motion type with iTNC530

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

is it possible to use nurbs as the motion type with CSE?

 

The code looks like :

 

SPLX=8.9012 Y29.7546 Z-2.7789 K3X=-0.0457 K2X=-0.467 K1X=1.0615 K3Y=0.1146 K2Y=-0.3197 K1Y=-2.0662 K3Z=-0.3381 K2Z=0.6531 K1Z=-0.5376

 

Thank you!

 

Best wishes,

Viktor

9 REPLIES

Re: CSE - nurb motion type with iTNC530

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!

First of all - Heidenhain not supported NURBS spline, your example is spline like y=Ax**3+Bx**2+Cx+D for each axis XYZ. It possible, I did a same for VERICUT -

Re: CSE - nurb motion type with iTNC530

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

And I see some mistake in your records SPLX=, right SPL X Y Z KX.......

Re: CSE - nurb motion type with iTNC530

I just loaded the out of the box sim01_mill_3ax_tnc_mm and simulated a nurbs path.

What issues are you having?

Mark Rief
Retired Siemens
Highlighted

Re: CSE - nurb motion type with iTNC530

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

NO COMMENTS

SPL_DOC.png

 

 

SPL.png

Re: CSE - nurb motion type with iTNC530

I saw the same error message when I switch from tool path to machine code simulation. 

I set the operation to Sinumeril Spline output, and used the post from sim01.

 

Mark Rief
Retired Siemens

Re: CSE - nurb motion type with iTNC530

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks for your feedback.

 

Now the syntax is correct, but of course a parsing error.

It seems like there is no interpretation ootb for the Heidenhain spline right now...

 

Best wishes from Hamburg,

Viktor

Re: CSE - nurb motion type with iTNC530

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Syntax is incorrect now, see a page from Heid Programming Manual in my previous message.

 

You can use CSEPreprocessLine to avoid parser error for SPL word, and - to assign coefficient values for some Q-vars. Then - open new subroutine and calc all intermediate points for spline.

 

It possible.

Re: CSE - nurb motion type with iTNC530

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

with the actual OOTB Parser and TNC Driver spiles are not supported with CSE.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE - nurb motion type with iTNC530

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Learn online





Solution Information