Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE origin load

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hello,

 

I have a CNC control that use this sintax to load origin:

 

Loadzero="xyz"

 

xyz is the mcs name in Nx cam.

 

Anyone have some idea how to use this sintax in Sinumerik CSE machine simulation?

 

Thanks

Emilio

6 REPLIES 6

Re: CSE origin load

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Emilio,

 

I hope I understood you correctly.

The command LoadZero="xyz" is similar to Fanuc/Sinumerik G53?

 

If so you have to customize the parser and add later the created metacode to the CCF/MCF file.

 

Thomas

Re: CSE origin load

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Yes Thomas you have understood well.

 

But the origin name is not always the same. It dipend by mcs name.

 

Customer use nx 10.0.3, probabily I don't have the possibility to edit parser...

Re: CSE origin load

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Emilio,

 

if you know the variaty of possible names then you can also use CSEPReprocessLine.

To make it simple you can replace the csys string to "G53".

Use the forum search how to use it. There are some threads about it.

 

Thomas

Re: CSE origin load

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hi Thomas,

 

I know PreProcessLine method.

 

I'm trying to use but I have parse error after replace.

 

See the pictures.

 

Emilio

 

Re: CSE origin load

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Emilio

 

the problem are the " inside ""

It is needed to work with \ like

replaceSubstr("LoadZero=\"G54\"",strLine,"G54")

 

To allow using / it is needed to change the way the internal CSE parser is working set it here:

CSE-Parser.png

 

Hope that will help

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE origin load

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Hello Thomas,

 

it work well.

 

Many thanks!!!

 

Emilio

Learn online





Solution Information