Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE simulator horizontal boring machine

Experimenter
Experimenter

Dears, I work on simulator of 3 axis (X, Y and Z) machine with rotary table (B axis) with Sinumerik 840D operating system. I need to create cse driver (adjust existing cse driver). The machine has W axis coaxial with Z axis. W axis and Z axis are not used for simultanious motion. W axis is used as additiont to Z axis. Could someone give me any advice how to set coaxial axis in machine configurator, please? Thank you.

Jan Oliverius

1 REPLY 1

Re: CSE simulator horizontal boring machine

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Olli,

 

there is an existing NC Simulation sample shipped with NX. It´s the SIM17 machine, a horizontal machine tool with W axis. The W axis is compensated based on a value written in NC Code. Maybe it helps for your project.

 

..\mach\resource\library\machine\installed_machines\sim17_vertical_turnmill_dualchannel\cam_setup\sim17_turnmill_setup_sinumerik_mm.prt

 

Thomas

Learn online





Solution Information