Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - soft limit check rotary axis - NX11

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi everybody,

 

we have now some problems with soft/hard limit check for rotary axes.

The problem appears while using activateSoftLimitCheck() in a tool change subprog for example. Without the command everything works fine.

 

You can start a sim08 sample and after the toolchange you wont get a soft limit alarm after nc line like "G0 A190".

 

I dont get it...

 

Regards, Viktor

3 REPLIES 3

Re: CSE - soft limit check rotary axis - NX11

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Viktor,

 

which version are we talking about?

I checked the latest (dev) version and everything works as expected.

 

Thomas

Re: CSE - soft limit check rotary axis - NX11

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

we use NX 11.0.2.7 MP4, because of the IPW problems following in next MPs :/

 

2018-06-11 08_53_51-ConmatiX - NX CAM 11 SHARE - Fertigung - [sim08_mill_5ax_cam_sinumerik_mm.prt (G.png2018-06-11 08_54_05-ConmatiX - NX CAM 11 SHARE - Fertigung - [sim08_mill_5ax_cam_sinumerik_mm.prt (G.png

Regards, Viktor

Re: CSE - soft limit check rotary axis - NX11

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi Viktor,

I checked the NX1102 too and can verify the problem. This problem has been fixed in NX1201 and later versions.
When it´s critical open a GTAC call for it.

Thomas

Learn online





Solution Information