Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - thread-turn CYCLE97

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everybody,

 

I'm using NX10.02.6 and need to simulate the thread-turn operation CYCLE97.

An error "Method IsEqualObject was called with wrong number of arguments" prevents the simulation.

 

What could be the reason?

 

Thank you very much!

 

Best wishes from Hamburg

Viktor

2 REPLIES 2

Re: CSE - thread-turn CYCLE97

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Victor

 

it would be very helpful to know which command inside the cycle97 occurs this error message.

 

ThomasF

Re: CSE - thread-turn CYCLE97

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

there is only the error massage above named.

I solved this problem with customizing the CYCLE97.SPF ...

 

Best wishes

Viktor

Learn online





Solution Information