Cancel
Showing results for 
Search instead for 
Did you mean: 

CSE - turret with 2 channels

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi everybody,

 

I want to start a discussion Smiley Happy

 

We have a machine tool with 4 channels. The turret can be used in channel 1 or 2.

For us the right way is to swith the channel for every operation or tool.

 

2017-09-12 08_28_45-Werkzeugträger_1.png

2017-09-12 08_37_06-ConmatiX - NX CAM 10.03 SHARE - Fertigung - [Test_CAM_Benzinger_Plansee_V2.prt (.png

 

What do you think? What would you do?

 

Regards, Viktor

 

 

5 REPLIES 5

Re: CSE - turret with 2 channels

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Victor, that will be a cool discussion :-)

 

I like to better understand the use case.

 

You say the turret (holding tools) will be driven either by channel 1 or channel 2. That means different NC code files (channels) will drive the tool from that turret; is that correct. Can you share a picture of that machine tool?

 

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE - turret with 2 channels

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

you're right, that's correct.

The turret is used for the main and counter spindle. And both spindles have an own channel.

 

There are many ways to get the channel informations. In my opinion a clear way is to be based on the real machine. One pocket, a device and then the option to choose a channel to work with.

 

We develop a Benzinger Take 5.

 

2017-09-12 11_00_48-benzinger_take5_2007.pdf - Adobe Acrobat Reader DC.png

 

Regards, Viktor

Re: CSE - turret with 2 channels

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Victor, understood the Take 5. In that case how you suggested to set up the ONT should work.

 

Thomas

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: CSE - turret with 2 channels

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Thomas,

 

it works fine, we found it out Smiley Happy

 

But is it a good way?

Our customer think another method is good. Perhaps we take two turret devices, one for channel one and another device for channel two.

In this way we get problems with tool devices, for example a dual tool holder.

 

Regards, Viktor

Re: CSE - turret with 2 channels

Siemens Phenom Siemens Phenom
Siemens Phenom
Hard to say what is the best way, at least one which works ;-)
Sure two turrets might be easier for the visibility inside the ONT, but then you need to find a workaround for the dual tool holders, also not perfect.

As this is not a "normal" machine tool there is not THIS ONE way to do it.
The good think is that it can be solved with NX.
Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information