Cancel
Showing results for 
Search instead for 
Did you mean: 

CSEPreprocessLine with ""

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!

 

For Siemens controller (CTX1250) I have one problem - for part transfer I use FIXEDSTOP subroutine, for example:

 

FIXEDSTOP(Z3, 0, 0.2, 345.56.......), where first parameter - STRING. But - when I define this proc in subroutine - PROC ( STRING[32] AXIS_NAME, REAL ....) - I have error message about problem with paeser line.

 

FIXEDSTOP("Z3", 0, 0.2, 345.56.......), - no error messages.

 

And my first idea was replace FIXEDSTOP(Z3, to FIXEDSTOP("Z3", but - I cannot use "....

Any advises?

 

 

5 REPLIES

Re: CSEPreprocessLine with ""

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Maybe this data type shouldn't be a STRING, but AXIS?

 

axis.png

 

...I'm not sure, but just guessing

Marek Pawlus, NCmatic

Production: NX 11.0.2
Development: C#, Tcl/Tk, CSE

Re: CSEPreprocessLine with ""

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi YuriThomas,

 

I don´t see a problem. I tested the following code without any problems? What do you expect?

 

ThomasF

ENX_DEVunitfeindCCFDev_NX11_245_SIM16HEADCORRECTIONwntx64kitsmachresourc_2016-03-15_09-34-41.png

Re: CSEPreprocessLine with ""

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I've been looking for an example of CSEPreprocessLine.  Can you tell me where to find it?  I assume it will automatically get processed if it is present???

 

Thanks in advance

George

 

George Bennett
All NX versions
W7 Ultimate
Dell Precision M6700
Spirit of Innovation

Re: CSEPreprocessLine with ""

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi George,

 

attached is a PDF with all information you need. Let me know if you need further information.

 

Note: CSEPreProcessLine is a mighty function BUT be careful and use it only when there is no other way. The more processed code in the function is the more suffering the Perfomance!

 

ThomasF

Re: CSEPreprocessLine with ""

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thank you Thomas. Much appreciated.
George
George Bennett
All NX versions
W7 Ultimate
Dell Precision M6700
Spirit of Innovation

Learn online





Solution Information