Cancel
Showing results for 
Search instead for 
Did you mean: 

CSEPreprocessLine

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!

I use CSEPreprocessLine, working. But - only for one substitution..

How I can use this method for few cases? For example, I want to change "XA"->"X1=" and "YA"->"Y1="?

 

Thanks!

6 REPLIES 6

Re: CSEPreprocessLine

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Yuri,

 

I hope this help you.

 

Best regards,

 

2yuri.JPG

Re: CSEPreprocessLine

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello, I will relly apreciate if you can share some info about how to ser this method.

 

My Email is ubaldo.garcia@idcae.com

 

Thanks,

Re: CSEPreprocessLine

Pioneer
Pioneer

Bringing this thread back from the dead because the subject line is most relevant.

 

Is there any way to use the CSEPreprocessLine method in NX10?

 

Thanks,

John

Re: CSEPreprocessLine

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Yes.

I think I used it for first time in NX 8.0 or 8.5.

it worked the same way as it does with present NX versions

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: CSEPreprocessLine

Siemens Phenom Siemens Phenom
Siemens Phenom

I was hoping the questions would die out ;-)

 

CSEPreprocessLine function can still be used. Also in NX10. But we don´t recommend to use it any longer due to the availability of the Python based parser.

 

How to use the CSEPrepro**** peeeeeeepp function is described above.

 

Keep in mind that each NC command in each Line will call this function! This has an impact to the overall system performance and it can have side effects you don´t want . I've seen horrible things done with that function. And I'd don´t want to know what else some people have done with it. 

 

Use it only in exceptional cases and when you know what you´re doing. In all other cases we suggest to go with the Python approach.

 

Thomas

 

 

Re: CSEPreprocessLine

Pioneer
Pioneer

Thanks Thomas,

 

I didn't see the method in either CCF by default, so I added it - but it didn't seem to have any effect.

 

What about for Sinumerik? How can we customize the parser to accept a strange command?

Thanks,
John

Learn online





Solution Information