Cancel
Showing results for 
Search instead for 
Did you mean: 

CYCLE800 ERROR

Pioneer
Pioneer

Hi,

 

I need your help. CYCLE800 give me an error.

 

My program

 

1.JPG

Error

4.JPG

 

I created CUST_800.SPF file to my working directory to subprog.Content was taken from catalog.

5.JPG

 

I put "CUST_800" "to main.ini" file.

6.JPG

 

I put "CUST_800" program manager explorer.

2.JPG

 

Also I put _N_CST_DIR to win10 system variable.

3.JPG

 

No response.

 

Where have I made mistake? I use standart "SinumerikSL_Cycles_47_SP2_HF1.cyc".

 

 

 

 

 

3 REPLIES 3

Re: CYCLE800 ERROR

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

"I put "CUST_800" "to main.ini" file." --> this is not necessary. This subprog is called from within cycle800.

Both files are included in SinumerikSL_Cycles_47_SP2_HF1.cyc file and usable.

 

The cust_800 you are using here is very old and not in sync with the included version in cyc file. So I suggest to remove your cust_800 file from Program Manager.

 

Thomas

 

 

Re: CYCLE800 ERROR

Pioneer
Pioneer

Hi Thomas,

 

I have already removed CUST_800 from main.ini file and program manager.When I got to simulation, I have taken same error.

 

I am new in machining configuration. Probably I damaged commands. I have not tried sim8_5axis mach. I have just judged to return original sim8 mach.

 

This machine might be working cycles.

 

Thank you so much to reply.

Re: CYCLE800 ERROR

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi,

sorry I don´t have any idea why you get this message. I tried to reproduce the problem with the sim08 nc simulation sample without success. Please try the same.

Thanks
Thomas

Learn online





Solution Information